Forta series actuators with IP65

Issue

Is it possible to order a Forta actuator with IP class 65?

Product Line

Field Devices

Environment

Forta series actuator

M400

M800

M1500

M3000

Cause

Some environments are requiring a higher than normal IP rating.

Resolution

Unfortunately the design of the Forta actuators are only IP classed to IP54. No IP65 version is available.

An additional weatherproof bag may be added to cover the actuator. However, such bags needs to be purchased from other sources as they are not part of our portfolio.