What are the mobile apps for Pelco HVR's/NVR's?

Issue

  • Can Pelco Mobile app work with any Pelco DVR, HVR or NVR?
  • Is a mobile client for smartphones such as iPhone, BlackBerry, Android and Symbian devices available?

Product Line

Pelco Video Management

Environment

  • Pelco Mobile version 1.2.908
  • Pelco Video Management

Cause

  • Compatible DVR's, HVR's for Pelco Mobile.
  • View cameras on the recorder using handheld devices.

Resolution

The Pelco Mobile App v1.2.908 for Android and Apple devices is compatible with the following products:

  • DigitalSentry
  • Endura (SM5200) 

 

The DX Mobile app is available for:

  • DX4700/DX4800 v1.02 or higher
  • DX4700/DX4800 HD

 

The mobiDEOS Mobile App is available for:

  • DX8000
  • DX8100
     

The following models do not have Mobile App compatibility available:

  • DX3000, DX3100
  • DX4000, DX4100, DX4500, DX4600
  • DX4700/DX4800 non HD (version 1.01)*
  • DX7000, DX7100
  • DX9000, DX9100, DX9200
  • DVR5100 Series