Issue
Need a report of personnel that have not accessed the facilities in some specified time.
Environment
CyberStation
Cause
Documentation
Resolution
- Create a List View of the Personnel class
- Add desired columns (Name, Card Number etc)
- In the Qualifiers tab add the following advanced qualifiers
TimeEntered <= MyCyberStation\Date - xxx
where MyCyberStation is the name of the workstation object and xxx is a number that represents the number of seconds going back in time.
For example to generate a list view report of all personnel that have not accessed the facilities in a day enter the following qualifier
TimeEntered <= MyCyberStation\Date - 86400
(86400 is the number of seconds in a day)
For a qualifier for a month enter...
TimeEntered <= MyCyberStation\Date - 86400 * 30