Do we have an interface to the KNX/EIB protocol?

Issue

Do we have an interface to the KNX/EIB protocol?

Product Line

Andover Continuum

Environment

Continuum XDriver

Cause

Have a need to interface to a 3rd party device that is using the KNX/EIB protocol.

Resolution

Unfortunately, we do not have an interface to the KNX protocol. See this article for the XDriver interfaces that we do currently have available.

There are however, third party gateways available that may be able to help with this connectivity. They can provide the interface from KNX to one of the protocols that we do support such as Modbus or BACnet. Some examples that I've heard of people using in the past are below.

Loytec Gateway -> http://www.loytec.com/en/products/gateway-lon-bacnet-mbus-modbus-knx/444-lgate-950-universal-gateway
Fieldserver -> http://www.fieldserver.com/
Intesis Gateway -> http://www.intesis.com/eng/intesisbox_knx_frame_eng.htmI