The command GetMaxDigitalMag will return with the optical magnification if the camera does not support digital magnification

Issue

The "GetMaxDigitalMag" command to get the digital magnification gives a response of 0x or 1x. this is the optical magnification. You will see this on the Spectra HD line because the cameras have optical magnification and not digital.

Product Line

Pelco Cameras, Pelco Video Management

Environment

Any camera that does not support digital magnification, but has optical magnification type

Cause

This is due to the response giving a value but not having a way to give the correct value because the magnification is not true digital

Resolution

Engineering is looking at resolving in a future release