The folder name is included in the binding even when using relative path.

Issue

When doing a binding using relative path the folder name is included in the binding.
When clicking on the relative path button the binding looks like it should without the folder name but it is no possible to save it like that.

Product Line

SmartStruxure Solution

Environment

StruxureWare version 1.3

Cause

In the folder name a space was used.
 

Resolution

When taking away the space in the name the relative bindings looked like the should, no folder name in them.