How to set StorSave to performance mode on DSSRV-RD

Issue

Enabling the performance StorSave setting  significantly reduces the amount of dropped frames from the RAID card. 

Product Line

Pelco Video Management

Environment

DSSRV-RD

Cause

The default setting is "balanced" which bypasses a 512MB Cache

Resolution

1. On the DS-SRV, press Windows+R on the keyboard to open the Run command

2. In the Run command, type in “tw_cli” and press Enter

3. Click Yes on the User Account Control message

4. Type in “/c0/u0 set storsave=perform” and press Enter

5. Type in “y” and Enter to continue

6. Close the tw_cli window

7. Done