Issue
Which valves sizes are available for the V241 valve?
Environment
V241
Cause
Size specifications for V241 valves.
Resolution
The V241 valve is available in the following sizes:
DN15, DN20, DN25, DN32, DN40, DN50. Some of these are available in different Kvs values. For more information and details, please see the V241 data sheet available on the Extranet.