Issue
An R2 station is unable to communicate with any BACnet -MSTP controllers. Error in Standard Output Window:
"ERROR: Cannot open BACnet MSTP Driver
tridium.nre.DriverException: Cannot open Com5 [mstp]
at tridium.nre.vxworks.mstp.VxWorksMstpDriver.doOpen (bytecode 46)
at tridiumx.bacnet.services.link.mstp.MstpLinkService.start (bytecode 63)"
Product Line
TAC I/A Series
Environment
R2 station with BACnet/ MSTP trunk
Cause
The port specification is case-sensitive, and Com5 incorrectly includes lower-case characters.
Resolution
The MSTP port specification should be changed to COM5.