Issue
What is the process to order Esprit with IR Illuminators?
Product Line
Pelco Cameras
Environment
- ES30C-2N / ES31C-2N (24VAC) Models
- SMR1-1DYGZU
- IR229-Series
Cause
Process for purchase of Esprit and IR combination.
Resolution
To request the Esprit ES30C/ES31-2N with Pre-Installed Brackets to support two Iluminar IR229 Series Illuminators:
From Pelco:
- Select 24VAC Esprit Model.
- At time of Esprit order: Request SMR1-1DYGZU
- Installation Guide view.
SMR1-1DYGZU: Is designed to integrate up to two iluminar IR229-Series Infrared illuminators that follow the positioning and full 360 rotation of the Esprit Series camera. SMR is to add Dual IR Bracket to Esprit.
- Click Here for Bracket Explosion. (IR lamps illustrated as reference only and are not supplied by Pelco)
- Click Here for view of SMR specification sheet.
From IIuminar Inc:
- Request IR229 Series. Click Here to view Specification Sheet to IR229 Series and additional information.