AS supports network authentication via Radius Server (IEEE 802.1X)?

Issue

Does the Automation Server support network authentication via Radius Server (IEEE 802.1X)?

Product Line

SmartStruxure Solution

Environment

SmartStruxure Site

Cause

AS supports network authentication via Radius Server (IEEE 802.1X)?

Resolution

Remote Authentication Dial In User Service (RADIUS) is a networking protocol that provides centralized Authentication, Authorization, and Accounting (AAA) management for computers to connect and use a network service. RADIUS is a client/server protocol that runs in the application layer, using UDP as transport.

The RADIUS server is usually a background process running on a UNIX or Microsoft Windows server.

RADIUS serves three functions:

  • to authenticate users or devices before granting them access to a network,
  • to authorize those users or devices for certain network services and
  • to account for usage of those services. 

SmartStruxure does not support the RADIUS protocol.