Is there a diagram available connecting a CM9760-KBD Intelligent Keyboard to a CM9700-CC1 over Pelco Fiber?

Issue

CM9760-KBD keyboard is not communicating to a CM9700-CC1 over a fiber connection.

Product Line

Pelco Matrix

Environment

CM9700-CC1 all versions

CM9760-KBD all versions

Pelco Fiber all versions

Cause

Communication has not been established.

Resolution

Please see the attached diagram of a CM9760-KBD Intelligent Keyboard to a CM9700-CC1 over Pelco Fiber.

 

NOTE: if using FTV series fiber this will not work for this application.