What is the maximum number of configurable zones which can be created for a Digital Sentry system?

Issue

What is the maximum number of configurable zones which can be created for a Digital Sentry system?    

Product Line

Pelco Video Management

Environment

  • Digital Sentry versions 4.x - 7.x.x
  • Discontinued Digital Sentry hardware
  • DSSRV
  • ENC5416
  • DS NVs

Cause

Creating and configuring multiple zones for a Digital Sentry system. 

Resolution

There is no limit built into the Digital Sentry software for the number of Zones that can be created in DS Admin, however each Zone created and enabled will require system resources.