After rebooting the DVR5100DVD Hybrid Video Recorder it will not complete the boot process.

Issue

DVR5100DVD Hybrid Video Recorder will not boot up.

Product Line

Pelco Video Management

Environment

DVR5100 all versions

Cause

DVD disk is in the disk drive.

Resolution

1. Power unit down by holding in the power button for 5 seconds.

2. Power unit on by pressing power button for 1 second.

3. Watch the VGA screen, if you see the following.

4. Check the DVD drive and remove the disk.

5. Select the restart button in the lower left corner.

6. Unit will now boot up normally.