How is a camera assigned to a monitor to display when the CM9700 Matrix System boots up?

Issue

Need a particular camera to display on a monitor when the CM9700 Matrix starts up.

Product Line

Pelco Matrix

Environment

CM97xx Matrix System all versions

Cause

Wrong camera displayed on monitor.

Resolution

1. Log into the Pelco System Manager program, default user and password is Admin/Admin.

2. Select the monitor tab.

3. In the start camera column use the drop down menu to add the camera to the monitor

which will appear at system boot up.

4. Save and export the configuration and load on the CM9700-CC1. Use Lessons Learned

article LL#10699 for instructions on exporting the configuration files.