What are the default text onscreen positions for a CM9700 Matrix System Manager version 9.03.032?

Issue

Default settings have been change, would like to revert back.

Product Line

Pelco Matrix

Environment

CM97xx Matrix Systems version 9.03.0xx

Cause

Default text positions have been altered.

Resolution

The X coordinate is the starting point of the horizontal position of the on-screen text.

The Y coordinate is the vertical position of the on-screen text.

 

Default Positions for CM9760 and CM9765

X coordinates 1-24

Y coordinates 1-11

Alarm Text (X=1) (Y=5)

Camera Name (X=1) (Y=10)

Camera Number (X=1) (Y=9)

Monitor Name (X=1) (Y=1)

Time and Date (X=1) (Y=11)

 

Default Positions for CM9770 and CM9780

X coordinates 1-24

Y coordinates 1-25

Alarm Text (X=1) (Y=12)

Camera Name (X=1) (Y=23)

Camera Number (X=1) (Y=22)

Monitor Name (X=1) (Y=1)

Time and Date (X=1) (Y=24)