How to print a displayed video image on the DX Series Client?

Issue

How to print a displayed video image on the DX Series Client?

Product Line

Pelco Video Management

Environment

  • DX4000
  • DX4100
  • DX4500/DX4600
  • DX4700/DX4800
  • DX8000
  • DX8100
  • DX Series Client

Cause

Require a paper record of a video snapshot.

Resolution

  1. On the toolbar, click the Live icon 
     
  2. In the application window, click a view pane.
     
  3. In the timeline, select a date and time.
     
  4. On the Playback control, click Play .
     
  5. When the scene you want appears, on the Playback control, click Pause. The printer button becomes available.
     
  6. To print the image:
    • On the toolbar, click the Print icon . The Print dialog box appears.
    • Choose the printer settings, and then click OK. The image prints.