Issue
The CM9760-KBD Keyboard has a variable speed joystick with a zoom control knob for pan/tilt/zoom (PTZ) and dome control.
Product Line
Pelco Cameras, Pelco Matrix
Environment
CM9760-KBD - Programmable keyboard; 120 VAC, 60 Hz - all versions
Cause
Configuration and Programming
Resolution
OPERATING PTZ CAMERAS
The controls for PTZ cameras are located on the right side of the keyboard. If a PTZ camera is selected, “PTZ” appears on the top right corner of the LCD display.
The proportional joystick allows variable speed control. It gives you full control over the pan and tilt movements, from minimum to maximum speed. Speed is proportional to the amount the joystick is moved away from the center location.
Press while moving the joystick to enable high speed operation.
The joystick provides directional control only when a fixed speed PTZ camera is installed.
The various functions of a PTZ camera can be controlled as follows:
• Press to zoom in or out.
• Press to focus near or far.
• Press to open or close the iris.
It is possible to operate the joystick simultaneously with a lens function. The iris open and close key functions only with the appropriate lens fitted.