Issue
What Ethernet speed and duplex is supported by the MNB-1000?
Environment
MNB-1000
Cause
Specifications for IT infrastructure
Resolution
The MNB-1000 controller has auto-sensing Ethernet port (10/100 MB, half / full duplex) capabilities and are dependent on the network / switch to which they are connected. The MNB-1000 has the ability to auto negotiate with the Ethernet network on startup.