How to create a push button to launch an external application.

Issue

How to create a push button to launch an external application.

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Cause

Not sure how to open an external application from the Continuum Menu pages.

Resolution

To setup a button to run an external application, you can create a hotspot on a Menu page that when clicked, runs the application.

1. On the menu you want to add the button; right-click and select Edit.
2. Click and draw a rectangle.
3. Right click the rectangle and select Properties.
4. Edit the hotspot by giving a name, selecting Control to be Execute, select the application you want to run using the Open field, then tick "Make hotspot look like a windows button", and type a display label in the Button field.

5. Hit OK, then save and run the page.
6. Test that it works by pressing the button you just created.