What resolution and images per second (ips/fps) does Digital Sentry support connected to a Sarix IL10 Series IP camera?

Issue

What resolution and images per second (ips/fps) does Digital Sentry support connected to a Sarix IL10 Series IP camera?

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Digital Sentry software v7.3 or later
  • DS NVs v7.3 or later
  • DSSRV v7.3 or later
  • DSSRV2
  • Sarix IL10  v1.8.2.4.8310-O3.9119

Cause

Installing a new Sarix IL10 IP camera which connects to a Digital Sentry recorder.

Resolution

Primary Stream (1):

  • Resolution = 1280x720
  • Compression = H.264 / JPEG
  • IPS = 5, 10, 15, 25, 30

 
Secondary Stream (2):

  • Resolution = 640x352
  • Compression = H.264 / JPEG
  • IPS = 5