Can an automation server be installed with a backup database without the need for Workstation?

Issue

Can an automation server be installed with a backup database without the need for Workstation? 

For example, can a backup database be installed on a USB stick that is programmed to 'auto-run' when it is plugged into the automation server?

Product Line

SmartStruxure Solution

Environment

StruxureWare for Building Operations (all versions)

Cause

Customer works in the industrial refrigeration industry and his field personnel are primarily mechanics with limited pc knowledge.  Wants to use a stand-alone AS to control the refrigeration system.  Sites are mostly remote (several hours by car and/or flights). 

Wants to send programming changes, due to site installation changes, as a self-extracting and self-installing file on a USB stick.

Trying to avoid supplying the necessary laptops and Workstation training to the mechanics.

Resolution

This feature is not available.  Workstation is required for database administration.