DPUs stopped letting people through doors after upgrading the site from I/NET 2000 to the latest revision of I/NET Seven

Issue

DPUs stopped letting people through doors after upgrading the site from I/NET 2000 to the latest revision of I/NET Seven

Product Line

TAC I/NET

Environment

I/NET site with Access Control

Cause

DPUs stopped letting people through doors after upgrading the site from I/NET 2000 to the latest revision of I/NET Seven

Resolution

  1. Using Dbcreate, select “Verify existing database” and start the process. You will probably find errors or differences listed at the end of the verification check. (This probably caused the crash.)
  2. Using Dbcreate, select “Upgrade database” and start the process. Force I/NET Seven to upgrade the system. (The upgrade will attempt to repair the differences.)
  3. Once again, “Verify existing database” the database using Dbcreate. There should be “0” (zero) differences. If there are no differences, then the database is ready to be used in I/NET Seven.