Unable to set Units on an AI created in StruxureWare Building Operation Menta Editor

Issue

  • Unable to set Units on an AI created in Building Operation Menta Editor
  • The Units drop down list appears but is blank

Product Line

SmartStruxure Solution

Environment

SmartStruxure (all revisions)

Building Operation Menta Editor 

Cause

Menta Editor gets the units from Building Operation WorkStation.  If the Menta Editor is launched from the Start menu then there is no connection to WorkStation and units will not be displayed in Menta Editor. This is a known issue which will not corrected.

Resolution

Menta Editor gets the units from Building Operation WorkStation, so all Menta applications should be opened from within the Workstation by right clicking on the "ProgrammableXenta" object and selecting Edit.