Issue
Which pockets are included with the different size meters?
Environment
Kamstrup
Heat meter
Flow meter
Cause
Different applications requires different sensor pockets.
Resolution
65mm pockets included up to DN20, 90mm pockets between DN25-DN80, 140mm pockets from DN100 and up.