How to determine the name of the configuration file that is running on the CM97XX-CC1 Central Processing Unit.

Issue

How to get the CM97XX-CC1 Central Processing Unit configuration file name in order to make changes to the programming or to restart the Matrix system.

Product Line

Pelco Video Management, Pelco Matrix

Environment

CM97XX-CC1 Central Processing Unit all versions

Cause

Unknown configuration file running on the CM97XX-CC1 Central Processing Unit.

Resolution

1. Connect VGA monitor and the appropriate PC keyboard to the back of the CM97XX-CC1 Central Processing Unit.

 2. Press ALT+N on the PC keyboard that is connected to the CM97XX-CC1 Central Processing Unit. The configuration file name will be displayed at the bottom of the diagnostic screen see example below.