The DF5S-SMKIT Installation Operation Manual figure 2 dimensions are incorrect.

Issue

When there is not enough room to install the DF5S Series back box in the ceiling, the back box can be attached to the surface of the ceiling. A special trim ring–the DF5S-SMKIT–hides the back box. The entire assembly (back box and dome) hangs down only 6 inches (15.24 cm) from the ceiling.

 

C1475M-C (9/08) Figure 2 shows incorrect radius and wiring hole measurements.

Product Line

Pelco Cameras

Environment

DF5S series enclosure

DF5S-SMKIT

Cause

Manual Correction

Resolution

Use the following drawing in place of the Figure 2 drawing in the manual: