Keyboard shortcuts for Sarix IP cameras

Issue

  • What motion does the Sarix camera detect.
  • What analytics does the Sarix camera detect.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • All Sarix models
  • Pelco Media Player
  • Microsoft Internet Explorer

Cause

Verify what motion or analytics the Sarix IP camera is detecting.

Resolution

Several keyboard shortcuts are available when viewing the primary stream on the live video page using Microsoft® Internet Explorer® and the Pelco Media Player. These keyboard shortcuts display different overlays on a video pane and provide quick access to a specific function.

 Keyboard Shortcuts

Keyboard Shortcut Function
SHIFT + A

Displays analytics information for the currently active behavior. If there is no currently active behavior, this keyboard shortcut has no effect.

SHIFT + M  Displays motion information for the current view.
SHIFT + S  Displays details about the live video such as image rate, resolution, and bit rate.
SHIFT + T  Displays the current date and time.

 

 

 

 

 

 

Note: These keyboard shortcuts are not available when viewing video with Quicktime®  Must have Pelco Media Plugin.