What is the DX4700/DX4800/DX4700HD/DX4800HD HDD installation order

Issue

What is the DX4700/4800/DX4700HD/DX4800HD HDD installation order

Product Line

Pelco Video Management

Environment

  • DX4700/DX4800
  • DX4700HD/DX4800HD

Cause

Installing a new hard drive, upgrading storage, replacing a failed drive

Resolution

NOTE: Hard disk drives are installed in a specific order at the factory. When removing an HDD, be sure to label the drive to ensure that it is reinstalled in the same location.

 

  1. HDD 1: Connects to the SATA 1 connector
     
  2. HDD 2: Connects to the SATA 2 connector
     
  3. Mounting Bracket A
     
  4. HDD 3: Connects to the SATA 3 connector
     
  5. HDD 4: Connects to the SATA 4 connector
     
  6. Mounting Bracket B
     

Related Articles
What Operating System (OS) does the DX4500/DX4600/DX4700/DX4800 Series hybrid video recorder (HVR) use?