Wavelength frequency of the FMCI-AF1 Series

Issue

What is the lighting wave frequency that the FMCI-AF1MM1ST is using for transmit and receive?

Product Line

Pelco Transmission & Power

Environment

  • FMCI-AF1MM1ST, FMCI-AF1MM1STM, FMCI-AF1SM1ST, FMCI-AF1SM1STM
  • FMCI-BF1MM1ST, FMCI-BF1MM1STM, FMCI-BF1SM1ST, FMCI-BF1SM1STM

Cause

Wavelength specification required

Resolution

The light frequency on the FMCI-AFIMM1st is 1310 for transmit and 1550 for receive the matching part FMCI-BF1MMiST will have transmitter 1550 and receive 1310.