Differences between the Model 1119T and the Card-View Plus (Card Access Control Data Entry)

Issue

What is the difference between the Model 1119T and the Card-View Plus (Card Access Control Data Entry)?

Product Line

TAC I/NET

Environment

I/NET Site

Cause

What is the difference between the Model 1119T and the Card-View Plus (Card Access Control Data Entry)?

Resolution

The Model 1119T has been customized to easily work with TAC�s I/NET software (INET 2000 and INET Seven). The unit has five modes of operation for the different functions it can perform. The modes are explained further in the Description and Operation sections of the owner's manual. It has a recessed mode switch-button to toggle between the different modes, and the display constantly shows an abbreviation indicating the mode currently in use. It includes a plug-in wall transformer to provide power.