Why do Pinpoint buttons appear differently when changing the Windows profile

Issue

Different Windows Users see the Pinpoint buttons differently.

Product Line

Andover Continuum

Environment

Cyberstation Pinpoint

Cause

Continuum uses the information from the Windows profiles to define the system appearance.

Resolution

In the Windows Display properties you can select the "Windows and Buttons" style for your profile, this will change the appearance of the standard buttons used within Pinpoint graphics.

For example:

Selecting Windows XP Style will look like:

 

 Selecting Windows Classic Style will look like:

 

 

Windows7 also has other styles available.