After copying sections of logic from one application to another the ability to connect pointers stopped working.

Issue

After copying sections of logic from one application to another the pointers from that logic won't connect to other objects and therefore show up as red lines.

Product Line

TAC I/A Series

Environment

WorkPlace Tech

Cause

Copying sections of logic from an older application has been known to cause this.

Resolution

To recover the application remove all objects and reference tags that exhibit the connection issue, compile the application and then re-create the deleted logic by pulling objects from the Shapes window.