Issue
It takes a lot of time to test each node in a database to verify that they are all truly online.
Environment
- NL220
Cause
Instead of checking each node in NL220 one at a time, a test can be performed that will check all nodes at one time.
Resolution
- Right click on the subsystem in the network tree of NL220
- Click on Nodes
- Make sure that "Recursive commands on subsystem" is checked
- Click on Network
- Click Test
NL220 will now go through the entire database and perform a test on each node.