How to configure motion sensitivity on the DX4500/DX4600?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to configure motion sensitivity on DX4500/DX4600?

Product Line

Pelco Video Management

Environment

  • DX4500
  • DX4600
  • Motion Sensitivity

Cause

  • Increase Motion Sensitivity
  • Decrease Motion Sensitivity

Resolution

  1. Click on Setup
     
  2. Click the Linking menu option. The linking options are displayed


 

      3.   Click Motion

      4.   Click the channel/camera name you want to configure

      5.   Click Sensitivity to configure. NOTE: The sensitivity settings are: OFF, 0 to 9 and HIGHEST. By default, the sensitivity is set to 5.

6. Confirm Area is mask in green for motion trigger. Note: Red will flash in area of movement.