What Matrix system is the CM9502-KBD compatible with?

Issue

What systems can I use the CM9502-KBD on?

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM9502
  • CM9501
  • CM9502-KBD

Cause

Application of CM9502-KBD

Resolution

The CM9502-KBD is designed for connection to the CM9502 and CM9501 Matrix System only.