How many watts are consumed by Endura encoders?

Issue

The number of watts used per encoder must be determined to calculate the power draw on a system.

Product Line

Pelco Video Management

Environment

  • Endura NET5404T video encoder
  • Endura NET5402T video encoder
  • Endura NET5401T video encoder
  • Endura NET5301T video encoder

Cause

Not applicable.

Resolution

Model   Channels   Power   Power per Channel

NET5301T   1   8W   8W
SP04-140   2   8W   4W
NET5301T-I   1   14.5W   14.5W
NET5401T-I   1   10W   10W
NET5402T-I   2   13.5W   6.75W
NET5404T-I   4   26W   6.5W