Issue
What is the maximum system pressure for the meters?
Environment
Kamstrup
Heat meter
cool meter
flow meter
Cause
It is important to make sure that the system pressure does not exceed the maximum pressure specified for the components included.
Resolution
Depending on which meter is chosen, it is either 16 Bar (PN16) or 25 Bar (PN25). This is defined in the charts that are available here: