Can recorded video be played back using a CM9760 Intelligent Keyboard through the CM9700 Matrix Switcher?

Issue

Recorded video playback is desired using the CM9700 Matrix Switcher.

Product Line

Pelco Matrix

Environment

  • CM9760-KBD Keyboard version 8.45
  • CM97xx Matrix switcher version 9.03.0xx

Cause

Playback appears to be unavailable

Resolution

Recorded video is only an option when the CM9700 Matrix Switcher is interfaced with an Endura Recording solution using either the CM9700MDD-EVS or UDI5000-MTRX.