Activating and Deactivating Auxiliary Relay functions from the KBD300A

Issue

How to trigger auxiliaries/relays from the KBD300A.

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • KBD300A
  • CM6700 Matrix Series
  • CM6800 Matrix Series
  • Direct Mode (KBD300A, KBDKIT, Esprit with Wiper)

Cause

Procedure for operating the function of Auxiliaries/Relays from KBD300A

Resolution

For the CM6700:
Call up the relay number 01 or 02 auxillery.   F1 - F3 control only the auxiliaries built into the CM6700 SCU. These outputs can be programmed for momentary, keyed, latched, or alarm operation. Refer to the CM6700 manual for programming instructions.


F1/LATCH: Activate/deactivate auxiliary 1 relay.
F2/OFF:     Activate/deactivate switcher auxiliary 2 TTL output.
F3/MOM:    Activate/deactivate switcher auxiliary 3TTL output.
 

 

For the CM6800:
Call up the relay number 01 or 02 auxillery.   F1-F3 can address auxiliary functions on the CM6800 and on the REL2064 to provide additional points.


F1/LATCH: Enter the auxiliary number and press and release F1 to turn on an auxiliary (latching).
F2/OFF:     Enter the auxiliary number and press and release F2 to turn off an auxiliary (latching).
F3/MOM:    Enter the auxiliary number and press and hold down F3 to turn on an auxiliary (momentary). Release F3 to turn off the auxiliary.

Direct Mode:
In Direct Mode, F1-F3 have no function. LED shows PTZ camera receiver auxiliary number for two seconds after the AUX ON or AUX OFF key is pressed.

NOTE: The AUX ON and AUX OFF keys control the auxiliaries in PTZ camera receivers.
Enter the auxiliary number (ie 01,02) and press the AUX ON key to turn on. Repeat this function to turn it off. Hold, and then release for momentary functions.