Issue
How can an alarmed point be configured to close the currently active graphic before launching the graphic points alarm graphic.
Environment
- Pinpoint
- Alarm Graphic
Cause
Using the Display Graphic action on an Event View, it is necessary to have only one alarm graphic open at a time.
Resolution
Event Notifications provide for the launching of specific graphic panels when a point goes into alarm. No provision exists for closing having this alarm close the currently active graphic panel before it' launches its graphic.