Issue
Can Continuum Extended logging be configured on point with a Log Interval of less that 60 seconds.
Environment
- Continuum
- CyberStation
- Extended Logging
Cause
The project spec calls for extended logging of point with a 5 second log interval.
Resolution
While it is possible to configure extended logging points for intervals of 1 to 59 seconds, this is not recommended. Continuum should notify the operator that this is not recommended when the point is configured.