Issue
Message of BIOS version ready for download is displaying.
Product Line
Pelco Cameras
Environment
- Spectra III Series
Cause
Spectra III is experiencing an error detection of firmware update attempt.
Resolution
Spectra III should only display the message of "Bios Version, Ready For Download" when attempting to update the camera's firmware via IPS-CABLE. The message is prompted briefly when updating is initialized from laptop.
If a Spectra III is displaying this message constant with no attempt of firmware update, It is recommended to send Spectra III in for Pelco Repair.
See LL#11086 for sending in product for repair.