Issue
Which sensors can be used if mounted directly into the pipe, without pockets?
Environment
Kamstrup heat cool flow meters
Cause
In some applications, sensors mounted directly into the pipe, without using pocket, is requested.
Resolution
Unfortunately, we do only recommend the sensors that are included with the meter package, or ordered as an option with longer cords. All are requiring pockets for proper mounting.