Spectra IV IP Alarms

Issue

What are the functions of the Spectra IV IP Alarms

Product Line

Pelco Cameras

Environment

  • SD4N Spectra IV IP Models
  • TXB-IP version 01.02.0018

Cause

Alarm status indication

Resolution

The Web page of the Spectra IV IP features an Alarm Panel. Lights indicate the status of the alarms set for the Spectra IV unit. A red light indicates that the alarm is active, a green light indicates that the alarm is inactive.

 

  • The alarms contact and actions are programmed within the Spectra IV 95 Preset Menu. Click on the OSD icon to prompt cameras 95 Preset menu.
  • The 23X models have one alarm input available. The 27X and 35X models have seven alarm inputs.
  • Click here to view the Spectra IV Alarm menu pages.
  • Click here to view the door panel alarm wiring terminals.