Issue
Need to know the connector genders to order the interconnecting ribbon cable.
Environment
DO-20 DM-20 DIO-20
Cause
Not in the documentation for the DO-20.
Resolution
All three have a female DB25 connector. Also, the interconnecting cable from the DM-20 to the DO-20 or DIO-20 is a straight-through 25 conductor cable.