NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
Unable to exit from the Menu on the Genex Multiplexer
Product Line
Pelco Cameras, Pelco Video Management
Environment
- MX4009
- MX4016
- Genex Series
Cause
How do you get out of the Program menu on the Genex Series Multiplexers
Resolution
To Exit out of the Genex Multiplexer menu, use the directional arrows located on the front panel:
- Press the Arrow Keys until the Cursor is on Exit and make sure Exit is flashing
- Press the +/- Button on the front of the Multiplexer