Issue
V282 is obsolete and a replacement valve is requested.
Environment
V282:
7218206000
7218210000
7218214000
7218218000
7218222000
7218226000
7218230000
7218234000
7218238000
7218242000
7218246000
7218250000
V241:
7214106000
7214110000
7214114000
7214118000
7214122000
7214126000
7214130000
7214134000
7214138000
7214142000
7214146000
7214150000
Cause
Obsolete valve needs replacement.
Resolution
The recommended replacement valve for valve model V282 is V241.
However, when so is done, pipe work will be necessary to adapt to installation with couplings and dimensions.