Mounting the WM2000 wall mount to the PP4348 parapet, rooftop mount.

Issue

Parapet mounting option for Sarix box camera with EH1512 enclosure.

Product Line

Pelco Cameras

Environment

  • WM2000
  • AH1000
  • AH2000
  • EA4348
  • PP4348

Enclosures

  • EH1512
  • EH3512
  • EH4700
  • EH5700 (requires AH2000)

Cause

Parapet, Rooftop mounting Sarix EH1512 enclosure.

Resolution

The WM2000 rear hole pattern aligns with the EA4348 adapter plate. The EA4348 allows mounting the WM2000 to the PP4348.

With the following combination of product, mounting to the PP4348 will be possible for any of the listed enclosures.

  1. WM2000
  2. AH1000 or AH2000
  3. EA4348
  4. PP4348