MPT9500 Connector pinout and type of connector

Issue

Pinout for RS485 on the MPT9500

Product Line

Pelco Video Management, Pelco Matrix

Environment

MPT9500

Cause

What is the pinout for the MPT9500 RS485 also what type of connector is it?

Resolution

The MPT9500 RS485 connector is a RJ-12

 

 

The pinout is as follows: